BridgeTransitionBuilderWidthDirectionOptions Enumeration¶
NXOpen.Features.SheetMetal.BridgeTransitionBuilder.WidthDirectionOptions is an alias for NXOpen.Features.SheetMetal.BridgeTransitionBuilderWidthDirectionOptions
-
class
NXOpen.Features.SheetMetal.
BridgeTransitionBuilderWidthDirectionOptions
¶ Bases:
object
Enum representing the width direction for the Bridge Transition. This enum applies only when the width type is
Features.SheetMetal.BridgeTransitionBuilderWidthOptions.Finite
. TheFeatures.SheetMetal.BridgeTransitionBuilderWidthDirectionOptions.Right
option indicates that the width is in the counter clockwise direction of flow of the start edge in the non-thickness face adjacent to it. TheFeatures.SheetMetal.BridgeTransitionBuilderWidthDirectionOptions.Left
option indicates the width is in the opposite direction.Enum Members
Enum Member Enum Member Description Left It means Bridge Transition width direction at point specified and fin direction are in opposite direction. Right It means Bridge Transition width direction at point specified and fin direction are in same direction. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-