BendTaperBuilderChainingType Enumeration¶
NXOpen.Features.SheetMetal.BendTaperBuilder.ChainingType is an alias for NXOpen.Features.SheetMetal.BendTaperBuilderChainingType
-
class
NXOpen.Features.SheetMetal.
BendTaperBuilderChainingType
¶ Bases:
object
This enum represents the chaining options for the bend taper.
Deprecated since version NX8.5.0: Use WebTaperType instead.
Enum Members
Enum Member Enum Member Description BendOnly Bend Only BendFace Bend and Face BendFaceChain Bend and Face Chain -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-