BendTaperBuilderBendTaperSides Enumeration¶
NXOpen.Features.SheetMetal.BendTaperBuilder.BendTaperSides is an alias for NXOpen.Features.SheetMetal.BendTaperBuilderBendTaperSides
-
class
NXOpen.Features.SheetMetal.
BendTaperBuilderBendTaperSides
¶ Bases:
object
This enum represents the taper sides options for the bend taper.
Enum Members
Enum Member Enum Member Description Both Both Sides Side1 Side 1 only Side2 Side 2 only Symmetric Symmetric. Side 1 = Side 2 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-