BendListItemBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
BendListItemBuilder
¶ Bases:
NXOpen.Builder
Represents a Sheetmetal Flat Pattern bend list item builder class.
This builder is used to edit the bend sequence ID and bend name of the bends in the bend list. BendListItemBuilder objects will be created and populated in the BendListBuilder when bend information of a flat pattern view is populated. User should never need to create or delete BendListItemBuilder object on its own. To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateBendListItemBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
BendID | Returns or sets the new bend id |
BendName | Returns or sets the bend name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BendID¶
-
BendListItemBuilder.
BendID
¶ Returns or sets the new bend id
-------------------------------------
Getter Method
Signature
BendID
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendID
Parameters: bendId (int) – New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendName¶
-
BendListItemBuilder.
BendName
¶ Returns or sets the bend name
-------------------------------------
Getter Method
Signature
BendName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendName
Parameters: bendName (str) – New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
Validate¶
-
BendListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.