AdvancedFlangeBuilderTypes Enumeration

NXOpen.Features.SheetMetal.AdvancedFlangeBuilder.Types is an alias for NXOpen.Features.SheetMetal.AdvancedFlangeBuilderTypes

class NXOpen.Features.SheetMetal.AdvancedFlangeBuilderTypes

Bases: object

This enum defines the type options.

Enum Members

Enum Member Enum Member Description
ByValue
ToReference
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.