SectionSurfaceBuilderTypes Enumeration¶
NXOpen.Features.SectionSurfaceBuilder.Types is an alias for NXOpen.Features.SectionSurfaceBuilderTypes
-
class
NXOpen.Features.
SectionSurfaceBuilderTypes
¶ Bases:
object
This enum represents the current types of section surface methods
Enum Members
Enum Member Enum Member Description EndsApexShoulder ends apex shoulder EndsSlopeShoulder ends slope shoulder FilletShoulder fillet shoulder EndsApexRho ends apex rho EndsSlopeRho ends slope rho FilletRho fillet rho EndsApexHilite ends apex hilite EndsSlopeHilite ends slope hilite FilletHilite fillet hilite FourPointSlope four point slope FivePoint five point ThreePointArc three point arc TwoPointRadius two point radius EndSlopeArc point radius angle arc PointRadiusAngleArc point radius angle arc Circle circle CircleTangent circle tangent EndsSlopeCubic ends slope cubic FilletBridge fillet bridge LinearTangent linear tangent -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-