SectionSurfaceBuilderSectionMethodRhoEnum Enumeration¶
NXOpen.Features.SectionSurfaceBuilder.SectionMethodRhoEnum is an alias for NXOpen.Features.SectionSurfaceBuilderSectionMethodRhoEnum
-
class
NXOpen.Features.
SectionSurfaceBuilderSectionMethodRhoEnum
¶ Bases:
object
This enum represents the current types of section method for section methods with rho law
Enum Members
Enum Member Enum Member Description Rho rho law method LeastTension least tension method -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-