SectionSurfaceBuilderExConicType Enumeration¶
NXOpen.Features.SectionSurfaceBuilderEx.ConicType is an alias for NXOpen.Features.SectionSurfaceBuilderExConicType
-
class
NXOpen.Features.
SectionSurfaceBuilderExConicType
¶ Bases:
object
This enum represents the current modes of conic type section surfaces.
Enum Members
Enum Member Enum Member Description Shoulder Shoulder mode Rho Rho mode Hilite Hilite mode FourPointSlope Four Point Slope mode FivePoint Five Point mode -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-