SectionInertiaAnalysisBuilderTypes Enumeration

NXOpen.Features.SectionInertiaAnalysisBuilder.Types is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderTypes

class NXOpen.Features.SectionInertiaAnalysisBuilderTypes

Bases: object

The type of Section Inertia Analysis to be performed.

Enum Members

Enum Member Enum Member Description
ParallelSections Parallel Sections Type
SectionsAlongCurve Sections Along Path Type
ExistingSection Existing Section Type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.