SectionInertiaAnalysisBuilderSectionAxisNormal Enumeration

NXOpen.Features.SectionInertiaAnalysisBuilder.SectionAxisNormal is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderSectionAxisNormal

class NXOpen.Features.SectionInertiaAnalysisBuilderSectionAxisNormal

Bases: object

Slice direction in case of parallel section type of analysis.

Enum Members

Enum Member Enum Member Description
Xc Along X Axis
Yc Along Y Axis
Zc Along Z Axis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.