SectionInertiaAnalysisBuilderSampleMethod Enumeration

NXOpen.Features.SectionInertiaAnalysisBuilder.SampleMethod is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderSampleMethod

class NXOpen.Features.SectionInertiaAnalysisBuilderSampleMethod

Bases: object

Type of sampling method to be used in sections along curve type of analysis.

Enum Members

Enum Member Enum Member Description
ByDistance Sample according to Distance
ByNumber Sample according to Number of slices
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.