SectionInertiaAnalysisBuilderCoordSys Enumeration

NXOpen.Features.SectionInertiaAnalysisBuilder.CoordSys is an alias for NXOpen.Features.SectionInertiaAnalysisBuilderCoordSys

class NXOpen.Features.SectionInertiaAnalysisBuilderCoordSys

Bases: object

The coordinate system associated with the analysis.

Enum Members

Enum Member Enum Member Description
Absolute Absolute Coordinate System
CurrentWCS World Coordinate System
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.