SectionCurveBuilderSpacingType Enumeration¶
NXOpen.Features.SectionCurveBuilder.SpacingType is an alias for NXOpen.Features.SectionCurveBuilderSpacingType
-
class
NXOpen.Features.
SectionCurveBuilderSpacingType
¶ Bases:
object
Represents spacing type.
Enum Members
Enum Member Enum Member Description EqualArcLength Equal arclength spacing EqualParameterSpacing Equal parameter spacing GeometricProgressionSpacing Geometric progression spacing ChordalToleranceSpacing Chordal tolerance spacing IncrementalArclengthSpacing Incremental arclength spacing -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-