SectionCurveBuilderPlaneType Enumeration¶
NXOpen.Features.SectionCurveBuilder.PlaneType is an alias for NXOpen.Features.SectionCurveBuilderPlaneType
-
class
NXOpen.Features.
SectionCurveBuilderPlaneType
¶ Bases:
object
Represents section plane type.
Enum Members
Enum Member Enum Member Description Selected Planes are selected (not specified by one of the following methods) Parallel Set of planes parallel to a base plane Radial Set of planes radiating from a base plane PerpendicularToCurve Set of planes perpendicular to a curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-