ResizeCurveBuilderValueType Enumeration

NXOpen.Features.ResizeCurveBuilder.ValueType is an alias for NXOpen.Features.ResizeCurveBuilderValueType

class NXOpen.Features.ResizeCurveBuilderValueType

Bases: object

the option for radius or diameter

Enum Members

Enum Member Enum Member Description
Diameter
Radius
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.