ResizeChamferBuilderSectionType Enumeration

NXOpen.Features.ResizeChamferBuilder.SectionType is an alias for NXOpen.Features.ResizeChamferBuilderSectionType

class NXOpen.Features.ResizeChamferBuilderSectionType

Bases: object

the chamfer section types

Enum Members

Enum Member Enum Member Description
SymmetricOffset
AsymmetricOffset
OffsetandAngle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.