RadialDimensionBuilderValueOption Enumeration

NXOpen.Features.RadialDimensionBuilder.ValueOption is an alias for NXOpen.Features.RadialDimensionBuilderValueOption

class NXOpen.Features.RadialDimensionBuilderValueOption

Bases: object

the option for radius or diameter

Enum Members

Enum Member Enum Member Description
Radius
Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.