ProjectCurveBuilderProjectionOptionType Enumeration¶
NXOpen.Features.ProjectCurveBuilder.ProjectionOptionType is an alias for NXOpen.Features.ProjectCurveBuilderProjectionOptionType
-
class
NXOpen.Features.
ProjectCurveBuilderProjectionOptionType
¶ Bases:
object
Represents projection option type used when direction type is along vector
Enum Members
Enum Member Enum Member Description NotSet Represents None ProjectBothSides Represents Project Both Sides EqualArcLength Represents Equal Arc Length -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-