ProjectCurveBuilderDirectionType Enumeration¶
NXOpen.Features.ProjectCurveBuilder.DirectionType is an alias for NXOpen.Features.ProjectCurveBuilderDirectionType
-
class
NXOpen.Features.
ProjectCurveBuilderDirectionType
¶ Bases:
object
Represents direction method
Enum Members
Enum Member Enum Member Description AlongFaceNormal Represents Along Face Normal TowardPoint Represents Towards Point TowardLine Represents Towards Line AlongVector Represents Along Vector AngleToVector Represents Angle To Vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-