ProjectCurveBuilderArcLengthType Enumeration¶
NXOpen.Features.ProjectCurveBuilder.ArcLengthType is an alias for NXOpen.Features.ProjectCurveBuilderArcLengthType
-
class
NXOpen.Features.
ProjectCurveBuilderArcLengthType
¶ Bases:
object
Represents Equal Arc Length type
Enum Members
Enum Member Enum Member Description BothXY Represents Both X and Y FirstXThenY Represents First X then Y FirstYThenX Represents First Y then X XOnly Represents X only YOnly Represents Y only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-