PointSetBuilderSplinePointsType Enumeration¶
NXOpen.Features.PointSetBuilder.SplinePointsType is an alias for NXOpen.Features.PointSetBuilderSplinePointsType
-
class
NXOpen.Features.
PointSetBuilderSplinePointsType
¶ Bases:
object
The settings for the spline points definition.
Enum Members
Enum Member Enum Member Description DefiningPoints Points will be created at spline defining points. Knots Points will be created at spline knot points. Poles Points will be created at spline pole points. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-