PatchOpeningsBuilderTypes Enumeration¶
NXOpen.Features.PatchOpeningsBuilder.Types is an alias for NXOpen.Features.PatchOpeningsBuilderTypes
-
class
NXOpen.Features.
PatchOpeningsBuilderTypes
¶ Bases:
object
The method used to patch the opening
Enum Members
Enum Member Enum Member Description Quilted Patch with quilted patchwork of faces NSided Patch with N-sided surface area method Mesh Patch with through curve mesh ByDeletingEdges Patch by deleting edges and growing faces Extension Tangent edge extension method Notch Notch fill method Joggle Joggle fill method MoldWizard Patch with Mold wizard edge patch method BySuppression Patch by suppressing features -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-