PatchOpeningsBuilderOutputTypes Enumeration¶
NXOpen.Features.PatchOpeningsBuilder.OutputTypes is an alias for NXOpen.Features.PatchOpeningsBuilderOutputTypes
-
class
NXOpen.Features.
PatchOpeningsBuilderOutputTypes
¶ Bases:
object
Indicates what to output
Enum Members
Enum Member Enum Member Description SingleFeature Output one feature containing all patch sheet bodies MultipleFeatures Output one feature for each patch sheet body Sew Sew patch sheet bodies into target sheet body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-