PasteFaceBuilderPasteOptionType Enumeration¶
NXOpen.Features.PasteFaceBuilder.PasteOptionType is an alias for NXOpen.Features.PasteFaceBuilderPasteOptionType
-
class
NXOpen.Features.
PasteFaceBuilderPasteOptionType
¶ Bases:
object
represents the paste option which defines whether the tool body is additive or subtractive. The paste option can be determined automatically from the add or subtract attributes on the tool body, or manually for a tool body lacking the said attributes.
Enum Members
Enum Member Enum Member Description Automatic determined automatically from the ‘add’ or ‘subtract’ attributes on each tool body. Add each tool body will add to the target body. Subtract each tool body will subtract from the target body. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-