OvercrownBuilderOutputType Enumeration

NXOpen.Features.OvercrownBuilder.OutputType is an alias for NXOpen.Features.OvercrownBuilderOutputType

class NXOpen.Features.OvercrownBuilderOutputType

Bases: object

This enum represents the output type of Global Shaping Operation

Enum Members

Enum Member Enum Member Description
Sheet
Solid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.