OffsetSurfaceBuilderOrientationMethodType Enumeration¶
NXOpen.Features.OffsetSurfaceBuilder.OrientationMethodType is an alias for NXOpen.Features.OffsetSurfaceBuilderOrientationMethodType
-
class
NXOpen.Features.
OffsetSurfaceBuilderOrientationMethodType
¶ Bases:
object
Represents the type of orientation method. This is applicable only if the output output is
NXOpen.Features.OffsetSurfaceBuilderOutputOptionType.OneFeatureForEachFace
. The first enum value implies that the offset direction will be that of the surface normal whereas the second enum value implies that am interior position will be specified and the offset direction will be away from this pointEnum Members
Enum Member Enum Member Description UseExistingNormals SpecifyInteriorPosition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-