MoveFaceBuilderTypes Enumeration¶
NXOpen.Features.MoveFaceBuilder.Types is an alias for NXOpen.Features.MoveFaceBuilderTypes
-
class
NXOpen.Features.
MoveFaceBuilderTypes
¶ Bases:
object
the move face types, don’t use it until nx502
Enum Members
Enum Member Enum Member Description TranslateDirectionAndDistance Direction and Distance for moving the faces TranslateBetweenTwoPoints Move faces in the direction and distance defined by the two points RotateAboutAxis Move faces by rotating about an axis RotateBetweenTwoAxes Move faces by rotating the axis from the first to the second -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-