MoveEdgeBuilderEndFaceBehaviorType Enumeration

NXOpen.Features.MoveEdgeBuilder.EndFaceBehaviorType is an alias for NXOpen.Features.MoveEdgeBuilderEndFaceBehaviorType

class NXOpen.Features.MoveEdgeBuilderEndFaceBehaviorType

Bases: object

Represents the end face behavior.

Enum Members

Enum Member Enum Member Description
Extend
Morph
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.