MirrorBuilderCsysMirrorOptions Enumeration¶
NXOpen.Features.MirrorBuilder.CsysMirrorOptions is an alias for NXOpen.Features.MirrorBuilderCsysMirrorOptions
-
class
NXOpen.Features.
MirrorBuilderCsysMirrorOptions
¶ Bases:
object
the Coordinate System mirror options
Enum Members
Enum Member Enum Member Description MirrorXAndY Mirror X and Y and derive Z MirrorYAndZ Mirror Y and Z and derive X MirrorZAndX Mirror X and Z and derive Y -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-