MidSurfaceByFacePairsBuilderTrimmingOptionType Enumeration

NXOpen.Features.MidSurfaceByFacePairsBuilder.TrimmingOptionType is an alias for NXOpen.Features.MidSurfaceByFacePairsBuilderTrimmingOptionType

class NXOpen.Features.MidSurfaceByFacePairsBuilderTrimmingOptionType

Bases: object

trimming options

Enum Members

Enum Member Enum Member Description
AdvancedTrimming Advanced trimming
BodyBasedTrimming Body based trimming
TrimtoSide1withNoExtension Trim to master
SkipTrimming Skip trimming for replacement sheets
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.