MidSurfaceByFacePairsBuilderSurfaceType Enumeration

NXOpen.Features.MidSurfaceByFacePairsBuilder.SurfaceType is an alias for NXOpen.Features.MidSurfaceByFacePairsBuilderSurfaceType

class NXOpen.Features.MidSurfaceByFacePairsBuilderSurfaceType

Bases: object

midsurface options

Enum Members

Enum Member Enum Member Description
Standard Default surface creation method
Side1 Use side 1 faces as mid sheet
Offset Use offset
CloudOfPoints Cloud of points
Large Use single largest surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.