MidSurfaceByFacePairsBuilderPairingStrategyType Enumeration

NXOpen.Features.MidSurfaceByFacePairsBuilder.PairingStrategyType is an alias for NXOpen.Features.MidSurfaceByFacePairsBuilderPairingStrategyType

class NXOpen.Features.MidSurfaceByFacePairsBuilderPairingStrategyType

Bases: object

pairing strategy

Enum Members

Enum Member Enum Member Description
Progressive Progressive thickness is used
Thickness Find all faces within search distance
Manual Manual pairing process
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.