MeshTransformerBuilderStepCountValue Enumeration¶
NXOpen.Features.MeshTransformerBuilder.StepCountValue is an alias for NXOpen.Features.MeshTransformerBuilderStepCountValue
-
class
NXOpen.Features.
MeshTransformerBuilderStepCountValue
¶ Bases:
object
Step count enum value for converting to actual count number
Enum Members
Enum Member Enum Member Description Number8 Step count 8 Number16 Step count 16 Number32 Step count 32 Number64 Step count 64 Number128 Step count 128 Number256 Step count 256 Number512 Step count 512 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-