MatchedReferenceBuilderTypes Enumeration¶
NXOpen.Features.MatchedReferenceBuilder.Types is an alias for NXOpen.Features.MatchedReferenceBuilderTypes
-
class
NXOpen.Features.
MatchedReferenceBuilderTypes
¶ Bases:
object
MatchedReference block type
Enum Members
Enum Member Enum Member Description Curve single curve or edge Face single face or datum plane CurveCollector curve collector or edge collector FaceCollector face collector Section section Point point Vector vector Object general geometry such as the target body and the tool body for copying unite feature BodyCollector body collector Csys csys Plane plane Axis axis Undefined default type for feature name lable -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-