MatchEdgeBuilderTypes Enumeration¶
NXOpen.Features.MatchEdgeBuilder.Types is an alias for NXOpen.Features.MatchEdgeBuilderTypes
-
class
NXOpen.Features.
MatchEdgeBuilderTypes
¶ Bases:
object
Match Edge match types. The match to datum type is deprecated in NX7.0.
Enum Members
Enum Member Enum Member Description MatchEdgeToEdge Edge to Edge match type MatchEdgeToFace Edge to Face match type MatchEdgeToCurve Edge to Curve match type MatchEdgeToDatum Edge to Datum match type. This type deprecated in NX7.0. Use NXOpen.Features.EdgeSymmetry
feature instead.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-