MatchEdgeBuilderPoleMovementConstraintEnumType Enumeration¶
NXOpen.Features.MatchEdgeBuilder.PoleMovementConstraintEnumType is an alias for NXOpen.Features.MatchEdgeBuilderPoleMovementConstraintEnumType
-
class
NXOpen.Features.
MatchEdgeBuilderPoleMovementConstraintEnumType
¶ Bases:
object
Pole movement type
Enum Members
Enum Member Enum Member Description WCS Along WCS X/Y/Z direction View Along view Vector Along user defined vector Normal Normal Project Project Inherit Inherit FixStart Fix start FixEnd Fix end StartAndEnd Fix start and end -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-