MatchEdgeBuilderEdgeConstraintType Enumeration¶
NXOpen.Features.MatchEdgeBuilder.EdgeConstraintType is an alias for NXOpen.Features.MatchEdgeBuilderEdgeConstraintType
-
class
NXOpen.Features.
MatchEdgeBuilderEdgeConstraintType
¶ Bases:
object
Edge constraint type
Enum Members
Enum Member Enum Member Description Linked Linked, available for end edge only Free Free Perpendicular Perpendicular IsoU Iso u IsoV Iso v Linear Linear -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-