LinearDimensionBuilderOrientationOptionType Enumeration¶
NXOpen.Features.LinearDimensionBuilder.OrientationOptionType is an alias for NXOpen.Features.LinearDimensionBuilderOrientationOptionType
-
class
NXOpen.Features.
LinearDimensionBuilderOrientationOptionType
¶ Bases:
object
the option that controls whether the OrientXpress or whether the vector block Controls the orientation of the Linear Dimension
Enum Members
Enum Member Enum Member Description OrientXpress Orientation option using Orient Xpress Vector Orientation option using vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-