LatticeBuilderLatticeTypes Enumeration¶
NXOpen.Features.LatticeBuilder.LatticeTypes is an alias for NXOpen.Features.LatticeBuilderLatticeTypes
-
class
NXOpen.Features.
LatticeBuilderLatticeTypes
¶ Bases:
object
This enum represents the lattice types that are supported in NX.
SurfaceGraph and TetrahedronGraph are not currently supported.
Enum Members
Enum Member Enum Member Description UnitGraph SurfaceGraph TetrahedronGraph ConformalGraph -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-