LabelChamferBuilderChamferOrientType Enumeration

NXOpen.Features.LabelChamferBuilder.ChamferOrientType is an alias for NXOpen.Features.LabelChamferBuilderChamferOrientType

class NXOpen.Features.LabelChamferBuilderChamferOrientType

Bases: object

the option for chamfer orientation types

Enum Members

Enum Member Enum Member Description
Convex
Concave
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.