IsoclineCurveBuilderCurveTypes Enumeration

NXOpen.Features.IsoclineCurveBuilder.CurveTypes is an alias for NXOpen.Features.IsoclineCurveBuilderCurveTypes

class NXOpen.Features.IsoclineCurveBuilderCurveTypes

Bases: object

The option indicating number of curves to be created

Enum Members

Enum Member Enum Member Description
Single
Multiple
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.