HolePackageBuilderHoleDepthLimitOptions Enumeration¶
NXOpen.Features.HolePackageBuilder.HoleDepthLimitOptions is an alias for NXOpen.Features.HolePackageBuilderHoleDepthLimitOptions
-
class
NXOpen.Features.
HolePackageBuilderHoleDepthLimitOptions
¶ Bases:
object
Represents hole depth limit options.
Enum Members
Enum Member Enum Member Description Value Value limit options UntilSelected Until selected limit options UntilNext Until next limit options ThroughBody Through body limit options -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-