HelixBuilderLengthMethods Enumeration¶
NXOpen.Features.HelixBuilder.LengthMethods is an alias for NXOpen.Features.HelixBuilderLengthMethods
-
class
NXOpen.Features.
HelixBuilderLengthMethods
¶ Bases:
object
Method for defining the length
Enum Members
Enum Member Enum Member Description Limits Length by start and end limit Turns Length by number of turns -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-