GlobalShapingPointOffsetBuilder Class¶
-
class
NXOpen.Features.
GlobalShapingPointOffsetBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
The class used to define the points and offsets needed for the target point list.
To create a new instance of this class, use
NXOpen.Features.GlobalShapingBuilder.NewTargetPoint()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Offset | Returns the target point offset |
Point | Returns or sets the target point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Offset¶
-
GlobalShapingPointOffsetBuilder.
Offset
¶ Returns the target point offset
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Point¶
-
GlobalShapingPointOffsetBuilder.
Point
¶ Returns or sets the target point
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
GlobalShapingPointOffsetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.