GlobalShapingBuilderTargetCurveOrientationType Enumeration¶
NXOpen.Features.GlobalShapingBuilder.TargetCurveOrientationType is an alias for NXOpen.Features.GlobalShapingBuilderTargetCurveOrientationType
-
class
NXOpen.Features.
GlobalShapingBuilderTargetCurveOrientationType
¶ Bases:
object
Represents the orientation of the target curve(s) to the limit curves. With parallel option you can specify only one law. With the perpendicular option, you can specify multiple laws.
Enum Members
Enum Member Enum Member Description Parallel Target curve is parallel to the limit curves. Perpendicular Target curves are perpendicular to the limit curves. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-