GlobalShapingBuilderRadiusType Enumeration¶
NXOpen.Features.GlobalShapingBuilder.RadiusType is an alias for NXOpen.Features.GlobalShapingBuilderRadiusType
-
class
NXOpen.Features.
GlobalShapingBuilderRadiusType
¶ Bases:
object
Represents radius options used.
Enum Members
Enum Member Enum Member Description Quintic Quintic method. A quintic curve is used to reduce the radius Radius Radius method. A true arc with tangent lines at the ends is used to reduce radius. This should be used when you know that the input is an edge blend or face blend -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-