GlobalShapingBuilderPointMethodType Enumeration¶
NXOpen.Features.GlobalShapingBuilder.PointMethodType is an alias for NXOpen.Features.GlobalShapingBuilderPointMethodType
-
class
NXOpen.Features.
GlobalShapingBuilderPointMethodType
¶ Bases:
object
Represents the point method type.
Enum Members
Enum Member Enum Member Description OffsetFromSheet Target point is offset from sheet PointDefined Target point is the given point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-