GlobalShapingBuilderDirectionMethodType Enumeration¶
NXOpen.Features.GlobalShapingBuilder.DirectionMethodType is an alias for NXOpen.Features.GlobalShapingBuilderDirectionMethodType
-
class
NXOpen.Features.
GlobalShapingBuilderDirectionMethodType
¶ Bases:
object
Represents the direction method type.
Enum Members
Enum Member Enum Member Description SameAsProjection Overcrown is same as projection direction NormalToSheet Overcrown is normal to sheet NormalToBase Overcrown is normal to base surface NormalToControl Overcrown is normal to control surface SpecifiedDirection Overcrown is user specified direction NotSet Overcrown has no direction specified -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-