GlobalShapingBuilderDeformationTypeValues Enumeration¶
NXOpen.Features.GlobalShapingBuilder.DeformationTypeValues is an alias for NXOpen.Features.GlobalShapingBuilderDeformationTypeValues
-
class
NXOpen.Features.
GlobalShapingBuilderDeformationTypeValues
¶ Bases:
object
Represents the deformation type.
Enum Members
Enum Member Enum Member Description ToPoint To point ToCurves To curves OpenRegion Open region WallDeformation Wall deformation Overbend Overbend MatchToSheet Match to sheet StretchToPoint Stretch to point StretchToCurve Stretch to curve RadiusReduction Radius Reduction BySurface - Old By surface method
ByCurve (10)Bend/Twist by curves Unknown Unknown deformation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.