GeomcopyBuilderTransformTypes Enumeration¶
NXOpen.Features.GeomcopyBuilder.TransformTypes is an alias for NXOpen.Features.GeomcopyBuilderTransformTypes
-
class
NXOpen.Features.
GeomcopyBuilderTransformTypes
¶ Bases:
object
user input transform types.
Enum Members
Enum Member Enum Member Description BetweenLocations between two point or csys locations Mirror mirror about a plane Translation translation along a direction Rotation rotation about an axis AlongCurve along a path Offset offset -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-